ACTION#.CONDITION
Description
This keyword defines the condition to test the action source for. If the value is 0 (always), then no test is performed and the condition always passes.
The available values of this parameter depend on the value of ACTION#.SOURCE. If the source is changed, the available range may be updated and the condition will be reset to default. Available conditions are:
Value | Description |
---|---|
0 | Always passes |
1 | Is false |
2 | Is true |
3 | Less than |
4 | Greater than |
5 | Rising Edge A rising edge is the transition of a digital signal from low to high. It is also called positive edge |
6 | Falling Edge |
7 | Rises above threshold |
8 | Falls below threshold |
9 | Rising Edge (triggers on high at start) |
10 | Falling Edge (triggers on low at start) |
11 | Is Equal To |
12 | Becomes Equal To |
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
Depends on ACTION#.SOURCE |
Default Value |
0 (always) |
Data Type |
Integer |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.